This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G07: May I have some confirming Item for SN74LVC1G07 ?

Part Number: SN74LVC1G07


Dear SIR :

May I have some confirming Item for SN74LVC1G07DCK ?

According to SN74LVC1G07DCK Pin 1 is NC. (Not connected) .

Is that meaning SN74LVC1G07DCK Pin 1 without any internal circuit and we can connect pin 1 and pin 2 together  (or any need consider)?

Thanks

  • Yes, the NC pin is not internally connected. You can route any signal or voltage on that pin that you would like.

    If this answers your question, please click the green "this resolves my issue" button, or reply to this message and I will continue to help.