Part Number: SN74LVT125-EP
Other Parts Discussed in Thread: SN74LVT125, SN74LVTH125, SN54AC244-SP, SN54LVCH244A-SP, SN74LVC2G126-EP
I need to drive a SPI clock bus signal from a microcontroller (with low drive strength/high output resistance) to 12 devices on a SPI bus. Due to the multiple devices, the trace length will end up being long relative to the electrical length of the ~ 2ns rising edge. Therefore I intend to use 50 ohm controlled impedance trace routing, and am looking for a suitable 3.3V buffer that can drive an end terminated 50 ohm line.
The LVT logic family seemed like a good choice based on the high drive strength, 32mA at 3V. What is the output (source) resistance for the SN74LVT125-EP Quad buffer? Since output resistance is not given in the datasheet, I attempted to estimate from VOH/IOH at Vcc = 3V specs, as follows:
Rout ~ (3V - VOH-min)/IOH = (3V-2V)/32mA = 31.25 ohms. Is this a good estimate for Rout, or not accurate?
Are there any other 3.3V logic families with lower Rout that I should consider? I looked at several other logic families but none seemed to have a higher drive strength. Can you suggest any other buffers/line drivers with low output resistance for driving a 50 ohm terminated line without a large voltage drop? With Rout = 31 ohm, my voltage drop into an end terminated 50 ohm line will reduce VOH to ~ 2V, too low if I'm operating with 3.3V supplies.
Can I connect the inputs and outputs of 2 of these buffers in parallel to reduce the output resistance?
Thanks, Ted