Other Parts Discussed in Thread: SN74ALS133, SN74LVC1G04, , SN74HC21
Hi Engineer,
We need to have 12 signals need to go through the AND gate logic output, see up to 4 channels and 2 inputs, such as the following two:
Which two chips are more advantageous?
Due to the compact space of the board, it is desirable to use a small package, as follows;
If you have other models, please help recommend it.
Thanks.
Elsa Duan