In SN74LVC8T245 ,Input transition rise or fall rate is showed below, as my case,VCCI=1.8V,that is to say the max rise time is 1.8*20=36ns? If the rise time of the signal into the part is 80ns,what will happen to the part?
1、 the output will not follow the input?
2、 The part will get hot?