Part Number: TXS0108E
Other Parts Discussed in Thread: TXB0108,
I have two issues that I am trying to resolve before proceeding with using this part. We were originally looking at using a TXB0108 due to the datasheet stating that there is a Vcc isolation feature which we need.
From the TXB0108 datasheet: VCC Isolation Feature – If Either VCC Input Is at GND, All Outputs Are in the High-Impedance State
I am wondering if the TXS0108 also has this VCC isolation feature, i.e. are the output high impedance when the device is powered off?
Second question is related to the OE pin, we are connecting a 1.5V FPGA I/O to 1.8V Microprocessor I/O with this part so our VCCA=1.5V and VCCB=1.8V. The issue is we would like to drive the OE pin from the microprocessor side which is 1.8V logic. Can the OE pin be driven from 1.8V I/O even though it is referenced to VCCA which in this case is 1.8V.