This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G80-Q1: Help to confirm the output status of SN74LVC1G80 after power down and then power up again

Part Number: SN74LVC1G80-Q1
Other Parts Discussed in Thread: SN74LVC1G80, SN74LVC2G74-Q1

Hi team,

This is Jessica.Glad to work with you.

Could you please kindly help to confirm the output status of  SN74LVC1G80 if we power it down and then power it up. SN74LVC1G80 output is connected with a MOSFET gate for customer application. As we can see from datasheet, it shows that the output of 1G80 initial state is unknow,  so we want to confirm with you after power up every time, if the output status is unknow ? if it is unknow then maybe the design of customer is not appropriate.

Thank you & Best regards

Jessica