Part Number: SN74LVC244A
Hello,
The item (as many other items of TI as I've noticed) datasheet declares the following:
"OE should be tied to VCC through a pullup resistor to ensure the high impedance
state during power up or power down; the minimum value of the resistor is determined by the current sinking
capability of the driver."
Is it necessary to connect the OEn to a pullup resistor? it requires some logic to pull it low after power up, which complicates the design.
What voltage value can be generated at the output if don't do so (can it damage the receiver device)?
Thanks,
Max