Hi Team,
My customer is using the SN74HC4060 to get a fixed frequency output.
The target frequency of the PIN3 output is 400ms (f~=41kHz), so they made the design as below:
according to above SCH, the output frequency should be 47.44kHz.
However, the actual RC output is 41.58KHz, measured by the OSC.
PIN3's output is 2.54kHz (394ms)
So here comes the problem:
why is there huge difference between the theoretical frequency value (47.44KHz) and the real test one (41.58KHz)?