This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: Pull-up Resister

Part Number: TXS0102

Hi Team,

I have a question on TXS0102.
Are unused pins connected to GND? Is it VCC connection?

Also, although internal pull-ups are made on the A side and B side, is it OK to pull up externally?
The customer's board already has a pull-up resistor mounted and can not be removed.
Therefore, I want to check if there is a problem with the operation even if the pull-up resistor is attached.
Customers want to pull up with 1.2kΩ.

Best Regards,
Ishiwata