This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: How many max frequency can the device support ?

Part Number: TXS0108E


Dear all

      In the datasheet, it said max data rate is up to 110Mbps, but I want to know the max frequency that the device can support ? Could you share me ?

  • Hello Went,
    The maximum data rate of 110 Mbps can easily be used to determine the maximum square-wave clock frequency that can be passed through any device.

    A clock is just passing a series of 1 0 1 0 1 0...... forever. Since it takes 2 bits for the period of the clock, the maximum clock frequency will always be exactly half of the data rate -- ie this device can support up to 55 MHz square wave clocks.

    Another way to look at it is through pulse width. You can determine the maximum pulse width by: tw = 1/datarate = 1/110Mbps ~= 9.09ns
    This helps if you are trying to use something other than a square wave -for example, a PWM signal. The minimum pulse width must be 9.09ns.

    If this answers your question, please click the green "this resolved my issue" button - otherwise, reply and I will continue to help.