Part Number: SN74AUP1G07
Hi,
I have a question about the absolute maximum rating of Io listed in the data sheet P.4.
In "Continuous output current", the max value is specified as ±20mA.
In "Continuous current through VCC or GND", the max value is specified as ±50mA.
Why is it specified as ±50 mA?
Since the SN74AUP1G07 is a 1-channel buffer, I think that ± 50 mA does not exceed if the load current is within ± 20 mA.
Best regards,
Yuto Sakai