Part Number: SN74AHC14Q-Q1
One of our customer has a inquiry about SN74AHC14Q-Q1, please see the inquiry below:
The SN74AHC14QPWRQ1 is being used in multiple ECU's for automotive application, where the input voltages may be present when the supply rail is off (0 V). Our question is in regards to input current "Ii" specification which shows < 1 uA worst-case when Vi = 5.5 V or GND, and VCC = 0 V to 5.5V.
1) Where does the input current flow? Into the positive rail, ground, or outputs?
Based on the datasheet, it looks as if there is no input diode clamp to the positive rail which leads me to believe any current input would be directed to ground. I need to verify this though because if it does go to the positive rail, it will backfeed our 3.3V supply and turn on critical circuitry which must remain in a known-off state.
Thank you.
Regards,
Cedrick