Part Number: TXB0108
Other Parts Discussed in Thread: SN74AVC4T774
Hi
Hello, this is a schematic. Among them, 1.5V to 3.3V has not been working. 3.3V to 3.3V can sometimes work normally, sometimes not. When it can't work, it always outputs 3MHz clock and can't read FLASH. The attached picture is the timing diagram of the SPI mode for the FPGA configuration FLASH. I hope you can answer why 1.5V to 3.3V can't work. The FPGA bank voltage is 1.5V or 3.3V related configuration I changed. thank you!
Figure 1. FPGA configuration FLASH timing diagram
Figure 2. Can't read Flash_6MBPS_6MHz Clock
Figure 3. This can work_Sometimes Can't read Flash_6MBPS_6MHz Clock