Part Number: SN74LVCH16245A
Hello
Looking at SN74LVCH16245A (Buffer with HOLD option) datasheet, at Table 3 it states that for OEn pin at "1" the A, B buses are Isolated.
Does it mean that if I select DIR="0" (B --> A) and OEn = "1" than A bus pins will float at HighZ, or that A and B buses are isolated from each other and which values ("0" or "1") that were already "captured" over the A bus will keep their values regardless of changes at the buffer inputs?
I am asking from the point of view of the device which receives the A bus signals, will it fill during OEn="0" a valid value ("0" or "1") or the inputs of this device will start floating?
My motive for the above questions is that I was asked to check my card status when part of my blocks are powered down in standby mode.
I saw some of the inputs to the buffer will start floating (no pull up/ down) so I changed the buffer to the Hold option.
But on the output point of view, if the buffer is powered up and its receiver is powered down, a "1" at the buffer output will feed an input of a powered down device, an action which violates its Absolute Maximum Values. I order to be on the safe side I need the OEn pin to really float the A bus output pins towards the receiver. Is it so?
Thanks
Amnon