This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G08: please explain what is mean around Tr and Tf

Part Number: SN74LVC1G08


Dear,

I do not understand around TR and tf.

1.why need input ,I think ”input“ is unnecessary

2.why Tr,Tf have a max value. for example:

 if vdd is 3.3V ,tr max is 10ns/V from datasheet ,in this condition.if input signal rise and fall time (up to 1us/V) is very long ,in this case ,I have two question as follow:

1.actually,tr and tf of input signal is far beyond 10ns/V from datasheet,what will happen ? 

2.what is tr and tf of output signal?I want to know what is the meaning of tr max  existence?

Thanks!