Part Number: SN74LV00A
Hello,
I have a few questions regarding the SN74LV00A.
1) The SN74LV00A datasheet also lists specs for the SN54LV00A version but the SN54LV00A version is not listed as one of the orderable devices in the Package Option Addendum in the datasheet. Is the SN54LV00A version available? If so, what are the complete part numbers that can be ordered for the SN54LV00A version?
2) The SN74LV00A lists an operating free-air temp spec up to +125 degrees C. But this is a plastic part, and most plastic parts we are familiar with are only rated to +85 degrees C. Is the datasheet spec of +125 degrees C correct?
3) Is there any qualification data for the SN74LV00A with regards to +125 degrees C that TI can provide to us?
Thanks,
Scott