Part Number: CY74FCT16244T
Other Parts Discussed in Thread: 74ACT16244
Sir,
In one of the LED indication interface we are testing CY74FCT16244T for driving LED on the pannel @I=8mA.
Existing design latch can not driver the required current@5V that is why we have modified it with adding buffer CY74FCT16244T.
But It is observed that buffer CY74FCT16244T is not able to switch output above 4V output @5V input with no load at output.
Let us know any other option to replace CY74FCT16244T ,which can provide output 5V@8mA with <5V input .
Regards
Seema Joshi