Part Number: SN7407
Other Parts Discussed in Thread: SN74LVC07A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN7407
Other Parts Discussed in Thread: SN74LVC07A
hi dear .
again I did not get my answer!!!
Let's say we want to drive HCPL3120 (IGBT Driver) ,the sink for each driver is 12mA ,if all drivers are OFF then (12x6) =72mA
I want to know should I use 2 chips to drive 6 LED For IGBT Driver or One is enough?
Please Tell me if each buffer can sink up to 40 mA or the whole chip can sink up to 40 mA?
Regards.
Dave.
The 40 mA is for each channel.
Please note that there are other buffers that use less power. And the SN74LVC07A specifies the limits of both the per-pin current and the overall current (when using all outputs at the same time, each could drive 100 mA / 6 ≈ 16 mA).
Hey Dave,
My apologies for misunderstanding your question -- you were very clear and I guess I was just in a hurry.
Clemens is correct - the value there is per channel, but you shouldn't exceed 100mA total for the device -- which is what I meant by my first answer.
There is no specified Recommended Operating Condition value for the overall current, so it's the same as the Absolute Maximum Rating value.
Hey Dave,
There's no limitation in the datasheet, so there's no limitation. This is just my recommendation from my experience with these parts.
This part is ~60 years old -- I believe the original intent was for it to only drive 1 or 2 stages of additional logic, not to supply power to other circuits.
Thank dear
what is the difference between these chips?
74LS07,
74F07 ,
74LVC07,
74HC07 ,
7407
please explain it ,thanks!
Regards
Dave.
The difference is the logic family, i.e., the technology with which the chip was made.
The TTL family (SN7407) is the oldest one; it uses only NPN transistors, which means that the power consumption is comparatively high,
The later LS family adds Schottky diodes, which allows reduced power consumption at about the same speed as TTL.
LVC is a modern CMOS family; the static (when not switching) power consumption is approximately zero, at much higher speeds.
(TI never made a SN74F07 or SN74HC07, and those families have no benefits for your circuit.)