Part Number: TXB0108
Hi,
We are using TXB0108PWR in one of the boards where the signal is translating from 2.5V level to 3.3V.
The circuit diagram is as below:
We are driving the Signal SFP_TXdis (Pin 5) from the 2.5V side and on the scope we are able to see the level setting to 0V. But the Output side we have directly connected to connector and we do not have any component connected to the signal. But we see that the signal is at high level on the Pin 16.
Can anyone please let me know what could be the issue ?
Thanks & Regards,
Nanjunda M