This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104: TXB0104 Level Translator bidirectional

Part Number: TXB0104


Hi Team,

I would like to know if TXB0104 level translator can accept same voltage on both side A & B, I want to use it as a bidirectional buffer.

Can you check this issue?

Thanks,

Shlomi

 

  • Hi Shlomi,

    The datasheet recommends VCCA ≤ VCCB. So this will be fine as long as VCCB doesn't go lower than VCCA.

  • Please note that the TXB has very weak output drivers (this is required to allow automatic direction sensing; the other devices must have stronger drivers to allow them to override the voltage level). This means that the TXB is not suitable for most applications where you want a buffer.

    What is the actual problem you're trying to solve? Do you want more drive strength, or the ability do disconnect two buses?

  • Hi,

    The problem is that I need to drive bidirectional JTAG signal with long traces & wires, approx. 50 cm length..

    I didn’t find any other bidirectional buffer that I can use to drive this.

    In this case, I can use TXB on the weak side and TXA in the strong side?

    Thanks,

    Shlomi

     

  • Sorry; with "TXB", I meant the entire TXB0104 device. Both sides (A and B) have weak output drivers.

    It is not possible to increase the drive strength of bidirectional signals without a separate direction signal; if the pins on both sides have different voltages, how should the device know which one is to override the other?