Part Number: SN74F125
Whether SN74F125DR part can support 3.3V as a input
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74F125
Whether SN74F125DR part can support 3.3V as a input
Hi Keerthana,
This device has TTL thresholds meaning: if the signal is above 2 V, its considered a logic High and if the signal is below 0.8 V then its considered a logic Low. So a 3.3 V signal should work fine.