Part Number: TXB0108
Other Parts Discussed in Thread: TXS0108E, SN74LVC244A
Hello.
i'm using the TXB0108 to translate discrete signals from 5V (Port B) to 1.8V (Port A).
On the Driver side there is 5V via 100KOhm pull up ('1') or GND ('0') - push button triggered.
On the receiving side there is a FPGA input (no internal pull up).
On steady state there is 5V (via 100K pull up) on the driving side and once i push the button, there is GND on the driving side. this is the logic design.
'1' = button is open and '0' = button is close.
When i'm pushing the button, the output is latched to '0' and the input is latched to 200mV. this situation can't be changed until the next power up. translation doesn't work at all.
Please advise,
Gilad.