Part Number: SN74AHCT574
SN74AHCT574PW
Hi,
Please tell me how to calculate the power dissipation(mW) of this device.
best regrads
cafain
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74AHCT574
SN74AHCT574PW
Hi,
Please tell me how to calculate the power dissipation(mW) of this device.
best regrads
cafain
Hi, Ladisch san
Thank you for the information.
Please let me confirm in addition.
Power dissipation (Pd) is not described in the absolute maximum ratings of the data sheet.
Please tell me the Power dissipation (absolute maximum(Pd)) value as a device.
best regards
cafain
HI,
I thought as follows, is it wrong?
The allowable loss of PKG at Ta=25℃ is
When Rθja = 79.4℃/W of DW PKG,
At Ta=25℃, it is recommended that Ta (max is 125℃, so a rise up to 100℃ is considered acceptable.
(125-25)/79.4 = about 1.259 W, which is the power dissipation at DW-25℃ of DW PKG.
The allowable loss at Ta = 100℃ is
(125-100) / 79.4 = about 315mW
It will be.
Is the above idea OK?
best regards
cafain
Yes, this is the correct way to calculate the maximum power dissipation.
(At 5 V, and with all eight gates switching, the SN74AHCT574 dissipates 5.6 mW per MHz. In general, logic devices are not limited by their own operation.)