Part Number: SN74AHC244Q
Hi,
I have some question in use SN74AHC244Q.
3.3Vin for IC power supply, input is 5V square wave, output is 3.3V square wave.
Specification says that when 3V is supplied, the maximum effective level of VIL is 0.9V.
But when the VIL level is 1.4V, the output is also low. How should explain this? (Blue input, yellow output)
thanks.