This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0202: differences output levels

Part Number: TXS0202


I'm using TXS0202YZPR in the project. The A-voltage is 2.5V and B is 3.3V. When set high level on the D-(A) and D+(A), i see that D-(B) is 3.3V, but D+(B) is about 2.0V. I've tested it on two boards. What is the reason? Schematic:

This is D- 

D+ is:

Best regards.

  • There are two D+ pins and two D− pins. Which ones did you measure?

    The schematic is labeled "USB". Is this for USB, or IC-USB?

  • Sergey,

    As you have mentioned here in your post, the D+ and D- have differences in voltage levels and the scopeshots shown here in yellow is the B pins, correct?

    What is the difference on the D+(B) pins at the output as compared to the D-(B) pins. Is it measured at the same time or if possible measured one at a time to see if there is any difference in the readings?

    The TXS0202 device supports interchip USB which is different from the regular USB signals. The regular USB signals wouldnt need level translation as i know.

  • On the first measure the blue is D-(A) and yellow is D-(B). On the second blue is D+(A) and yellow D+(B). I use it to translate logic levels between mcu and usb-port.

  • What MCU are you using? What connector are you using on the USB port?

  • ShreyasRao said:
    As you have mentioned here in your post, the D+ and D- have differences in voltage levels and the scopeshots shown here in yellow is the B pins, correct?

    Yes, it is.

    The measurements were made at the same time. And this TXS0202 is also used for isolation the board from external voltage. Anyway I would like to understand the reason for this behavior of the chip.

  • Clemens Ladisch said:

    What MCU are you using? What connector are you using on the USB port?

    STM32F407VGT6. The connector is Molex 5015680307.

  • The TXB0202 works only with IC-USB (InterChip USB). The STM32F407xx does not support IC-USB. So you cannot use the TXB0202.

    The STM's USB pins already have the correct USB voltages, so you do not need a level shifter.

    You said you want isolation. What kind of isolation? If you want to disconnect the microcontroller from the connector, use analog switches. If you want to protect against overvoltage, use appropriate protection components (e.g., TVS diodes).