Hello guys,
One of my customers is considering using TXB0108 for their next products.
But the customer worries about IC breaking by input signal condition on A side and B side. Is there any prohibited condition of input shignal for the device?
Even if H or L signal is input to A side and B side at same time, is TXB0108 no damaged?
Could you please tell me whether the following input conditions are no problem or not?
1. A side = H level (DC), B side = L level (DC).
2. A side = L level, B side (DC) = H level (DC).
3. A side = H level (DC), B side = H/L clocking.
4. A side = L level (DC), B side = H/L clocking.
5. A side = H/L clocking, B side = H level (DC).
6. A side = H/L clocking, B side = L level (DC).
7. A side = H/L clocking, B side = H/L clocking.
Your reply would be much appreciated.
Best regards,
Kazuya.