Part Number: TXB0108
Other Parts Discussed in Thread: TXS0108E
Hello team,
I have a +3.3V FPGA connected to a +5.5V 75ALS160DW via the TXB0108, the interface signals being the 8-bit GPIB data bus.
I don't have any pullup/pulldown resistors on the either side of the TXB0108, and trace lengths will be short (low-capacitance).
The data rate will be relatively slow, but the FPGA and 75ALS160 may experience a condition where they are changing from driver to receiver, or vice versa, for a short period of time (controlled by software) where either both drivers may try to drive the A and B side to different levels at the same time, or both sides may temporarily "float" during this transition period (the "bus turn-around" period). The TXB0108 must be able to recover from this and not latch up or something like that.
Do you think TXB0108 is right part for the use case?
Best regards,