Part Number: TXS0104E
Other Parts Discussed in Thread: SN74AHC4066, SN74AXC4T774, TXB0104, TXB0304
Hi,
We are using the Texas part: TXS0104ERGYR for one of our applications. But it is not used for Level translation. We are using it as a buffer. 3.3V is fed to Both the voltages Vcca and Vccb. We are using enable signal to control the data flow. Default the enable is pulled low with a 10k resistor and the controller makes it high whenever necessary. The 4 channels are used for SPI lines Chip select, Clock, MOSI and MISO. We are using this part as a bridge between WiFi chip SPI lines and Flash Memory SPI lines using Enable as control. 'A' channel is given to Flash side and 'B' channel is given to WiFi chip side. Also the SPI lines from 'A' channel output is being shared to controller and FPGA. The SPI lines is not working when we mount the translator part on board. When the part is removed it is working fine. Not sure where am I missing.
Thank You.