Could you confirm that there are no problems with inductor constant and output capacitor constant?
Please refer to the "No 10" sheet.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
| Hi Expert. | ||||||||||||||
|
Is the pattern 2 too large for the inductor constant?
|
||||||||||||||
| Is the pattern 1 OK? " | ||||||||||||||
| "About the inductor constant | ||||||||||||||
| Follow Table 6 in the data sheet. , But | ||||||||||||||
| Please tell L value how much L value should actually be. | ||||||||||||||
| The conditions are as follows. | ||||||||||||||
| 1 Vout = 1.21 to 1.13 V | ||||||||||||||
| Vin = 3.8 to 4.2 V | ||||||||||||||
| Iout = MAX: 3079mA / TYP: 1500mA | ||||||||||||||
| Fs = 2.025 to 2.475 MHz [with SSC] | ||||||||||||||
| 2 Vout = 1.44 to 1.56 V | ||||||||||||||
| Vin = 3.8 to 4.2 V | ||||||||||||||
| Iout = MAX: 866mA / TYP: 343.9mA | ||||||||||||||
| Fs = 2.025 to 2.475 MHz [with SSC] | ||||||||||||||
| Previously, when asked about the inductor constant method, it was calculated by “ΔIL (max) <= 0.2 IOUT (max)”, and Pattern 1 was answered with 0.56 uH. | ||||||||||||||
| Pattern 2 selected 2.2uH according to the condition, but it is too large, so please tell L value how much L value should actually be. | ||||||||||||||
| Follow Table 6 in the data sheet. It can not be judged by the answer with | ||||||||||||||
| Could you show me the actual numbers? " | ||||||||||||||
| Best regards, | ||||||||||||||
| W.Makimoto | ||||||||||||||
| Hi Tanvee. | ||||||||||||||
| Is the pattern 2 too large for the inductor constant? | ||||||||||||||
| Is the pattern 1 OK? " | ||||||||||||||
| "About the inductor constant | ||||||||||||||
| Follow Table 6 in the data sheet. , But | ||||||||||||||
| Please tell L value how much L value should actually be. | ||||||||||||||
| The conditions are as follows. | ||||||||||||||
| 1 Vout = 1.21 to 1.13 V | ||||||||||||||
| Vin = 3.8 to 4.2 V | ||||||||||||||
| Iout = MAX: 3079mA / TYP: 1500mA | ||||||||||||||
| Fs = 2.025 to 2.475 MHz [with SSC] | ||||||||||||||
| 2 Vout = 1.44 to 1.56 V | ||||||||||||||
| Vin = 3.8 to 4.2 V | ||||||||||||||
| Iout = MAX: 866mA / TYP: 343.9mA | ||||||||||||||
| Fs = 2.025 to 2.475 MHz [with SSC] | ||||||||||||||
| Previously, when asked about the inductor constant method, it was calculated by “ΔIL (max) <= 0.2 IOUT (max)”, and Pattern 1 was answered with 0.56 uH. | ||||||||||||||
| Pattern 2 selected 2.2uH according to the condition, but it is too large, so please tell L value how much L value should actually be. | ||||||||||||||
| Follow Table 6 in the data sheet. It can not be judged by the answer with | ||||||||||||||
| Could you show me the actual numbers? " | ||||||||||||||
| Best regards, | ||||||||||||||
| W.Makimoto | ||||||||||||||
Hi Makimoto,
The inductor value should not be higher than the max value suggested in datasheet table7.3. According to me, a 600nH inductor is good enough and if you are concerned about the output ripple, it can be reduced using the output cap. If you would like to check different conditions I would recommend to use webench model which can help you to select the parameters for your design.
Best regards,
Tanvee
Hi Tanvee
Hi,
I would suggest following the section 10.1.3 in datasheet about the inductor selection. Normally the 0.47uH inductor is typically suggested for design but inductor value is selected according to the inductor current ripple. So, if you required low current ripple, I would suggest using higher inductor value but it should be in the range of datasheet specification. So, inductor value is flexible within range given in table7.3 in the datasheet but it depends on your application.
Best regards,
Tanvee
Hi,
Hi Makimoto,
First, the equation provided in the datasheet is for inductor ripple and the max inductor current calculation not for inductor value calculation. The ripple value change for each case and application. Your condition ΔIL (max) <= 0.2 IOUT (max) will not satisfy for all cases. For the second case, the ripple value will be higher and this is the main reason I was asking about inductor ripple requirement in your application. You can choose any inductor between 0.33uH to 0.9uH but the inductor ripple will change. I would suggest you can use 600nH but than ΔIL (max) <= 0.8 IOUT (max).
I am closing this thread and I would like to have a further discussion through email.
Best regards,
Tanvee