Part Number: SN7406
Other Parts Discussed in Thread: SN74LS06
The two ICs in questions are SN7406 and SN74LS06D. They both claim to have a High-Level output voltage of 30 Volts, but according to the function table of the SN74LS06D a TTL low would be Hi-Z, not a high output. Am I interpreting this wrong? The SN7406 looks like the function table would be:
|
Input A |
Output Y |
|
H |
L |
|
L |
H |
But I’m not sure if I’m misinterpreting the Y=Abar
On Page 8 of the SN74LS06D there’s the following function table.
The SN7406 has the following logic diagram on sheet 2.
Thanks,