I bought 4 of the chips from Mouser and none of them work. They said to try to get help here. I'm not sure why.
I already own one of the 74HC595 chips and it works good. I built a circuit to test it. Then when I put the new chips in, they didn't work.
Are some chips just bad or am I doing something wrong? I have positive and ground connected to pins 16 and 8 respectively. I have pin 13 output enable tied to ground. I tied pin 10 high, and put my clock to pin 11. Serial pin 14 I have connected to a momentary push button switch that is pulled down to ground with a 10k resistor until it is pushed, then it goes to the positive rail. All of the Q data pins are connected to 330 resistors then to the positive leads of LEDs to test.
This configuration works fine with the 74ls595 chip I got with a Virulos Arduino kit, but not with the 595's I got from Mouser. Any suggestions about what the problem may be, or should I just have Mouser send me 4 new ones or order from a different company? I thought it may be my clock pulse at first, but the data sheet I have says that there is not maximum clock value associated with this, so the 200 ns pulse I have set on my 555 timer should be working.
Thanks