Other Parts Discussed in Thread: SN74AXC4T774
Hello,
I have a TXS0108E for converting logic from/to 1.8V & 3.3V.
Please see below interface details.
I need help to resolve following issues:
- The SCK signal as soon as connected to CODEC side, the clock gets severely distorted. Not sure why?
- What I noticed is, if SCK signal from TXS is not connected to CODEC then SCK(at 3.3V side) does not have severe distortion. I suspect that the CODEC I am using has active pull-up on SCK(another other signals) and due to which TXS is misreading about which end is driving?
- In fact, I read the TXS0108E datasheet but could not find information showing how direction of the signal is automatically chosen?
Request you to help me resolve this interfacing issue.
Regards,
Krunal