This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF vs TXB vs TXC

LSF TXB TXC Abbreviation ?

How Auto sensing bidirectional is recommended in medical applications ?

Which of the families are recommended ? why ? which are widely used ?

  • Hi Gowtham,

    Please refer to the FAQ on this:

    These are generic translation devices and we do not have specific families for medical or safety applications. We do have the -Q1 which are qualified for automotive applications.

    Depending on the interface, channels, applications, any of the families can be considered.

  • Hi Shreyas,

    Thanks for your information on the comparison of LSF vs TXB vs TXC .

    Can you also provide more comparison with respect to technical parameters/specifications ? also cost comparison for any one common spec?

  • Family

    AXC

    AVC

    LVC

    Class

    Direction   Controlled

    Uni-Directional & Direction Controlled

    Direction   Controlled

    Interfaces supported

    Push-Pull

    Push-Pull

    Push-Pull

    VCC (V)

    .65 - 3.6

    1.2 - 3.6

    1.65 - 5.5

    Drive Strength (mA)

    12

    12

    32

    FMAX (MHz)

    190

    190

    150

    Max Bits

    8

    32

    16