This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ACT04: About connection between outputs in the same package of SN74ACT04

Part Number: SN74ACT04


Hello,

I am designing the gate drive circuit of FET. (Use FET : BSS316N  Ciss : 100pF)

I am considering using two NOT gates in the same SN74ACT04 in parallel for high-speed switching.

Is it possible to connect the outputs of two NOT gates in the same package?  (Circuit Example 1)

Or is it better to place a resistor to prevent short circuit as in Example 2?

Best regards,