Other Parts Discussed in Thread: SN74CB3T3245, SN74LVC245A, , SN74LVC244A
Dear expert,
As shown in the datasheet 6.3 section. When VCCA=3.3V and VCCB=5.5V, the high-level voltage VIHB(min)=3.85.
I want do confirm whether B port can support both 5V and 3.3V input signal when VCCB=5V and VCCA=3.3?
What is the input threshold level when VCCB=5V and VCCA=3.3?
Best regards,
Dylan Zheng