This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2T45: SN74LVC2T45

Part Number: SN74LVC2T45


Hi, 

Could you please let me know the pin to pin skew for SN74LVC2T45 and also to part to part skew information for the same part. 

Thanks and Regards

Raja

  • The difference in delay between the individual channels on an individual part  is referred to as channel-to-channel skew or output skew. This is not covered as a datasheet parameter.

    However we have a guarantee for all of our logic devices to limit output skew to 1ns. Keep in mind that this applies to a single unit with all driving inputs connected together and the outputs switching in the same direction while driving identical specified loads.

    Here is the what to expect for typical max skew based on technology. These are not guaranteed though:

     - TTL = 800ps
     - Bicmos  = 500ps
     - CMOS is 250ps

    AVC and LVC devices are CMOS

    There is no guarantee on part to part skew either, however if they are from the same batch then typically they should also be limited to 1ns part to part skew.

    Thanks!

    -Karan