I was hoping TI can suggest some parts to me.
I need a simple 3.3V to 5V logic lever shifter. And it must have an EN pin to force high z.
Unidirectional. 3.3V input logic 5V output logic. Output should be push pull since signal will be up to but no more than 10MHz.
Only 1 channel needed. Would like to have a single channel but max 4 channel option to keep the part size down.
I found this one (TXS0102), but i'm sure there are many more options out there. There is just too many options to sift through myself, i'm sure i'm missing many good options that maybe be cheaper than this one.
A better option is something small and cheap like this from ON Semi. M74VHC1GT125DF2G. Do you have a cross for this?
Thanks for the help