Part Number: SN74ABT245B
Hello,
customer want to sink 28mA current on 5 channels (sum 135mA). Is this ok? Do he has to take care on the layout?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74ABT245B
Hello,
customer want to sink 28mA current on 5 channels (sum 135mA). Is this ok? Do he has to take care on the layout?
Regards, Holger
Hi Holger,
The ratings given in the datasheet are for each single pin and not for the sum of all the pins. When the output of a pin is low, it can sink 64mA according to the datasheet. This means there shouldn't a problem sinking 28mA when the device drives low.
Thanks!
-Karan