Other Parts Discussed in Thread: SN74AXC4T245,
Hi dear supporting team,
could you pls help provide the min height value of SN74AVC4T245PWR? customer need the data to choose the heat sink size properly. tks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi dear supporting team,
could you pls help provide the min height value of SN74AVC4T245PWR? customer need the data to choose the heat sink size properly. tks!
Hi Vera,
The package dimensions can be found at the end of the datasheet in the POA.
Hi Dylan,
No, for PWR package, there is only Max height information in d/s, no min data. Could you pls help double check? Tks!
Hi Vera,
Only the max is given as this is typically what is needed for maintaining proper clearance. Heat sinks aren't really something I expect to be needed with these types of devices, but if it's a full system heat sink then I can understand. I'd say there's typically a 10% tolerance on that value meaning the height could be 10% less than the max, but not greater.