This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
We understand that VOH is 4.4V(min) at VCC=5.0V, IOH=-16mA.
However, we would like to know Minimum VOH at VCC=5.0V and IOH= less than -16mA (so from 0mA to 15mA).
----------
[Q1]
Could you please let us know if you have “VOH vs IOH Graph at VCC=5.0V”?
If you don’t have that Graph, could you please let us know the trend of VOH?
(For example, If IOH decrease, VOH decrease so there is Linearity.)
[Q2]
Could you please let us know if you have “Calculation method of VOH”?
For example, if VCC=5V and IHO=0/4/8/12/16mV, VOH=xx/xx/xx/xx/xxV.)
----------
Regards,
Kanemaru
Hi Clemens-san,
Thank you for your prompt reply.
I have three questions.
----------
[Q1]
Trend of “VOH” is different depending on "VCC".
Is this a correct trend?
-When Vcc=3.0V and IOH increase(From 5mA to 8mA), VOH decrease(From 2.7V to 2.6V).
-When Vcc=4.5V and IOH increase(From 8mA to 16mA), VOH increase(From 3.7V to 3.8V).
----------
[Q2]
We would like to know “VOH = VCC − 0.6 V × (IOH / −16 mA)”.
If IOH=-8mA and VCC=5V, VOH=2.2V
Is this result correct?
I am sorry if my interpretation is mistaken.
----------
[Q3]
We understand that Voltage drop at IOH=-40mA is around 1V.
Is my understanding correct?
And, could you please let us know the different of Line A and Line B?
----------
Regards,
Kanemaru
When VCC is larger, the gate-to-source voltage at the output transistors also is larger, so the transistors' RDS(on) and voltage drop become smaller.
VOH = 5 V − 0.6 V × (−8 mA / −16 mA) = 5 V − 0.6 V × 0.5 = 5 V − 0.3 V = 4.7 V
The graph uses the opposite sign for the current; Line A is VOL vs. IOL, Line B is VOH vs. IOH. (And 40 mA is outside the recommended operating conditions.)
Hi Kanemaru,
To add to to the info Clemens has provided, please refer to the FAQ below that covers this topic.
https://e2e.ti.com/support/logic/f/151/t/764984?tisearch=e2e-sitesearch&keymatch=faq%3Atrue
Hi Dylan-san,
Thank you for your response.
I understand. Thank you very much.
Regards,
Kanemaru