This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC125A: SN74LVC125A connect two output pin in parallel through 100 ohm to drive MOSFET

Part Number: SN74LVC125A


Hello E2E,

In order to get high driving current, Customer connect two output pin of SN74LVC125A  in parallel through 100 ohm  to drive external MOSFET.

Any concern on the connection?

Vgs,th is 0.45V - 1.2V. Could this connection fully turn ON MOSFET?

BR,

Jason