Part Number: TXS0108E
Hello.
Can two TXS0108E level shifters be connected in series?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gregory,
What is the application and what are the system voltage nodes?
The TXS0108 has smart pullup resistors which change between 4k or 40k depending on the input signal going high or low.
So, ideally yes, it can be done and as Clemens suggested the parallel combination will be higher; 4kohm || 4kohm. It is definitely higher current as compared to the 20kohm || 20kohm. Note that TXB is not recommended for back to back connection.