This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0102: Vref-A and Vref-B, Power up sequence

Part Number: LSF0102

LSF0102 support team

My customer is thinking using LSF0102 under the conditon of Vref_A = 1.8V and Vref_B = 3.3V like Figure 9 in the datasheet. And 1.8V rail is powered up after 3.3V rail is powered up.In this case, is the circuit as controlling EN pin to LOW needed until 1.8V rail is stabled? If YES, do you have the recommended circuit?

Thanks

Tamio