Part Number: TXB0104
Other Parts Discussed in Thread: TXS0108E, TXB0108,
Hello. We are debugging a design that uses the TXB0108. The part does not work in our application because of pull-ups internal to the part attached to the TXB0108. We solved the issue by using the TXS0108E and the interface is operational. However, a separate issue exists - VCCA=3.3V and VCCB=2.5V which violates the requirement that VCCA <= VCCB. The related question for the TXB0104 references internal diodes not shown on the block diagram. What are the consequences of this violation over industrial temperature and time?
Thank you