Other Parts Discussed in Thread: TXB0104, SN74AXC4T245, SN74AVC2T245, SN74AXC1T45, TXB0102
Hi :
I use the level conversion chip of TI. May I ask you some questions? Thank you!
1.TXS0104EPWR level conversion chip, VCCA connect 3.0V, level conversion chip will have leakage of 103uA.If the A1 channel of the level conversion chip is connected with a voltage greater than 3.0V, leakage of 2-3uA will occur,If I choose TXB0104, will there be leakage of electricity?
2.TXS0104 from the internal block diagram is a pull up resistance, VCCA on the power, all channels have voltage;And TXB0104 internal no pull-up resistance, is it true that after VCCA on, the corresponding channel no voltage output?
3.The current TXS0104 module TXD greater than A1 channel voltage, there will be leakage of 3uA, which will affect the PSM consumption of the module,Can you recommend a module TXD voltage will not leakage to level conversion chip IC?
My actual operation principle diagram is as follows, please guide me: