Hi,
I try to make TXB0104PW works with 3.3V SPI from STM32 and 1.8V IMU ICM-20948 but without success. I've re-soldered pins B1 - B4, provided input signals for A1-A4 (doesn't matter high, low or 50% duty pulses). there are no signals on output pins. 1.8 and 3.3 voltages are connected correct. Please see attached schematic.
Thanks,
Vasyl