Hi Team,
Please help me answer the follow question from my customer, thank you so much.
The table of “7.3 Recommended Operating Conditions” in the data sheet
has VIH = 2V and VIL = 0.8V when VCCI = 3V to 3.6V.
In this case, the duty will change, I think.
For example, when VCCI = 3V and High = 3V and Low = 0V Duty = 50% signal is input,
the output will be 51 to 52%.
Is Duty really changing between input and output?
How much is the error?
Best Regards,
Tom Liu