Part Number: SN74AVC2T45
Hello,
I have a requirement to design an externally configurable rs232/rs422 schematic.
Can i choose the component "SN74AVC2T45", for the above requirement.
I have an idea like:
By using two "SN74AVC2T45" devices, one for TX+ & TX- and other one is for RX+ & RX-.
Based on some I/o Control- i want to configure 232 or 422. Can i configure these devices either for RS232 or Rs422 using the IO controls?.
Thanks & Regards
Kalyan.