Other Parts Discussed in Thread: SN74LVC1G126
Team,
my customer needs a logic buffer (single gate) to drive the SDO line of an SPI connection. The SDO line has 100pF capacity (max).
The logic buffer needs to be able to drive this line.
How can I search for that capability?
The buffers I looked at so far can only drive 15 or 50pF.
Is there a solution at TI?
Thanks!