Part Number: CD4541B
Other Parts Discussed in Thread: CD4047B, CD4011B
The quiescent current is rated at 10uA max for 10V.
It is not clear to me if that rating is with the oscillator running or not.
I ask because my timer circuit is drawing 270uA while running and I want to be sure this is normal.
There is a note in the CD4541B data sheet referring to quiescent current.
it reads as follows:
With AUTO RESET enabled, additional current drain is
30μA (Typ), 350μA (Max) at 10V;
Does this note mean that with auto reset disabled, the quiescent current is 350 - 30 or 320uA typical?
Thanks..